GD3162 gate driver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

GD3162 gate driver

2,330 次查看
Akshat_VE02376
Contributor III

Hi NXP,
This is regarding the MODE2 register of gate driver 3162. What exactly is the correct way of writing to this mode 2 register? In our project we have observed several challenges in writing to this register:
1.When using unions to write to the MODE2 register bits, we are unable to write to this register

2.Now I'm writing directly the required value to this register after entering Configuration mode by setting CONFIG_EN to 1. Then in the data frame to be written, I'm keeping the CONFIG_EN bit as zero while writing. 

Now, that we are planning for BIST, this behavior of MODE2 can cause some issues. Please clarify what is the correct way of performing the write operation to this register.
This is the code snippet of my function :

FUNC (uint8, GD_CODE) GD316xCdd_Config_DaisyChain(void)
{
    uint8 GD316xCdd_ReturnStatus = E_NOT_OK;
    uint16 GD316xCdd_rxData[GD316xCdd_DEVCOUNT] = {0u}; /**< Buffer to store received SPI data */

    /* Initialize register settings to default values */
    GD316xCdd_mode1_settings.GD316xCdd_Data              = GD316xCdd_MODE1_DEFAULT_VALUE;
    GD316xCdd_mode2_settings.GD316xCdd_Data              = GD316xCdd_MODE2_DEFAULT_VALUE;
    GD316xCdd_config1_settings.GD316xCdd_Data            = GD316xCdd_CONFIG1_DEFAULT_VALUE;
    GD316xCdd_config2_settings.GD316xCdd_Data            = GD316xCdd_CONFIG2_DEFAULT_VALUE;
    GD316xCdd_config3_settings.GD316xCdd_Data            = GD316xCdd_CONFIG3_DEFAULT_VALUE;
    GD316xCdd_config6_settings.GD316xCdd_Data            = GD316xCdd_CONFIG6_DEFAULT_VALUE;
    GD316xCdd_config7_settings.GD316xCdd_Data            = GD316xCdd_CONFIG7_DEFAULT_VALUE;
    GD316xCdd_configAout_settings.GD316xCdd_Data         = GD316xCdd_CONFIGAOUT_DEFAULT_VALUE;
    GD316xCdd_statusMask1_settings.GD316xCdd_Data        = GD316xCdd_MSK1_DEFAULT_VALUE;
    GD316xCdd_statusMask2_settings.GD316xCdd_Data        = GD316xCdd_MSK2_DEFAULT_VALUE;
    GD316xCdd_reportMask1_settings.GD316xCdd_Data        = GD316xCdd_RMSK1_DEFAULT_VALUE;
    GD316xCdd_reportMask2_settings.GD316xCdd_Data        = GD316xCdd_RMSK2_DEFAULT_VALUE;
    GD316xCdd_OverTempThresh_settings.GD316xCdd_Data     = GD316xCdd_OT_TH_DEFAULT_VALUE;
    GD316xCdd_OverTempWarnThresh_settings.GD316xCdd_Data = GD316xCdd_OTW_TH_DEFAULT_VALUE;

    /* MODE1 register configuration */
    GD316xCdd_mode1_settings.Bits.GD316xCdd_AOUT      = GD316xCdd_MODE1_AOUT_TEMP_AND_SEC_QTY;
    GD316xCdd_mode1_settings.Bits.GD316xCdd_DSCH_CNTL = GD316xCdd_MODE1_DSCH_CNTL_PWM_FSSTATE;

    /* CONFIG1 register configuration */
    GD316xCdd_config1_settings.Bits.GD316xCdd_VCCUV_LATCH = GD316xCdd_CONFIG1_INTB_DISABLES_PWM;
    GD316xCdd_config1_settings.Bits.GD316xCdd_VCCUV_TH    = GD316xCdd_CONFIG1_UV_TH_10_0V;

    /* CONFIG3 register configuration */
    GD316xCdd_config3_settings.Bits.GD316xCdd_INTBFS = GD316xCdd_CONFIG3_INTB_INDICATES_FSENB_LOW;

    /* CONFIG6 register configuration */
    GD316xCdd_config6_settings.Bits.GD316xCdd_RTMONDLY = GD316xCdd_CONFIG6_RTMONDLY_2100_OR_1130N;
    GD316xCdd_config6_settings.Bits.GD316xCdd_VCCOV    = GD316xCdd_CONFIG6_VCCREG_18_0V;

    /* CONFIG7 register configuration */
    GD316xCdd_config7_settings.Bits.GD316xCdd_DESAT_TH = GD316xCdd_CONFIG7_DESAT_TH_11_25V;

    /* CONFIGAOUT register configuration */
    GD316xCdd_configAout_settings.Bits.GD316xCdd_AOUT_SEL = GD316xCdd_CONFIGAOUT_SEL_DESAT;

    /* MSK1 register configuration */
    GD316xCdd_statusMask1_settings.Bits.GD316xCdd_GSERRM = GD316xCdd_MSK1_Fault_NOT_MASKED;

    /* Enter configuration mode */
    GD316xCdd_ReturnStatus = GD316xCdd_Config_En_DaisyChain(TRUE);
    GD316xCdd_Config_Sts = TRUE;

    /* Writing configurations to GD316x registers */
    GD316xCdd_ReturnStatus = GD316xCdd_Wr_Reg_DaisyChain(GD316xCdd_spiAddrMode1, GD316xCdd_mode1_settings.GD316xCdd_Data);
    GD316xCdd_ReturnStatus = GD316xCdd_Wr_Reg_DaisyChain(GD316xCdd_spiAddrConfig1, GD316xCdd_config1_settings.GD316xCdd_Data);
    GD316xCdd_ReturnStatus = GD316xCdd_Wr_Reg_DaisyChain(GD316xCdd_spiAddrConfig3, GD316xCdd_config3_settings.GD316xCdd_Data);
    GD316xCdd_ReturnStatus = GD316xCdd_Wr_Reg_DaisyChain(GD316xCdd_spiAddrConfig6, GD316xCdd_config6_settings.GD316xCdd_Data);
    GD316xCdd_ReturnStatus = GD316xCdd_Wr_Reg_DaisyChain(GD316xCdd_spiAddrConfig7, GD316xCdd_config7_settings.GD316xCdd_Data);

    /* Enter normal run mode */
    GD316xCdd_ReturnStatus = GD316xCdd_Config_En_DaisyChain(FALSE);

    /* Reading and clearing fault status registers */
    GD316xCdd_ReturnStatus = GD316xCdd_Rd_Status1_DaisyChain(GD316xCdd_rxData);
    if ((GD316xCdd_rxData[0] > 0) || (GD316xCdd_rxData[1] > 0) || (GD316xCdd_rxData[2] > 0) ||
        (GD316xCdd_rxData[3] > 0) || (GD316xCdd_rxData[4] > 0) || (GD316xCdd_rxData[5] > 0))
    {
        GD316xCdd_ReturnStatus = GD316xCdd_Wr_Status1_DaisyChain(GD316xCdd_SPI_REG_DATA_MASK);
        GD316xCdd_ReturnStatus = GD316xCdd_Rd_Status1_DaisyChain(GD316xCdd_rxData);
    }

    GD316xCdd_ReturnStatus = GD316xCdd_Rd_Status2_DaisyChain(GD316xCdd_rxData);
    if ((GD316xCdd_rxData[0] > 0) || (GD316xCdd_rxData[1] > 0) || (GD316xCdd_rxData[2] > 0) ||
        (GD316xCdd_rxData[3] > 0) || (GD316xCdd_rxData[4] > 0) || (GD316xCdd_rxData[5] > 0))
    {
        GD316xCdd_ReturnStatus = GD316xCdd_Wr_Status2_DaisyChain(GD316xCdd_SPI_REG_DATA_MASK);
        GD316xCdd_ReturnStatus = GD316xCdd_Rd_Status2_DaisyChain(GD316xCdd_rxData);
    }
    return GD316xCdd_ReturnStatus;
}
0 项奖励
回复
3 回复数

2,309 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Akshat,

please download and check the GD31xx Driver Example Code for your reference. You can download it from the GD3162 product page, under the Software section.

Screenshot_1.png

In the example code, indeed extern union is used to write to Mode2 register. Please test the code and see if it will work for you. 

With Best Regards,

Jozef

0 项奖励
回复

2,297 次查看
Akshat_VE02376
Contributor III
Hi Jozef,
I already have this example code, but here mode2 is only used for unlocking the write operation by setting the CONFIG_EN bit to 1...There is no additional configuration/s done for MODE2. In my project I need to do other bit configurations for this register which is causing issue if I'm writing it in the same way in which other registers are written
0 项奖励
回复

2,286 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Akshat,

the issue might be not caused by the writing, but by the BIST you mentioned. Please download and refer to Errata sheet ER1. There is description of the BIST running issue and also a workaround. Please download the Errata sheet from the GD3162 product page, under the Secure section.

Screenshot_3.png

With Best Regards,

Jozef

0 项奖励
回复