Fully Connected layer conversion showing internal error in neutron converter in iMX95 Verdin

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Fully Connected layer conversion showing internal error in neutron converter in iMX95 Verdin

1,398 次查看
PoojaSk
Contributor II

Hi,

Tried converting classifier models such as InceptionV3, Resnet50 and Mobilenetv3Small using neutron converter targeting iMX95. On converting fully connected layer to ConvertFullyConnectedToConv, it is showing internal error. 

PoojaSk_2-1747980635221.png

 

PoojaSk_0-1747979255547.png

 

This is the fully connected layer which is not getting converted. But this layer does not violate any of the constraints mentioned in the section 5.9.7 FULLY_CONNECTED constraints of UG.

PoojaSk_1-1747979421074.png

 

 How can we fix this issue as I am unable to run any classifier with fully connected layer in iMX95 Neutron NPU.

0 项奖励
回复
2 回复数

1,207 次查看
varshilg
Contributor II

Hi Pooja,

I am also facing this issue that fully_connected layer not able to convert into neutron graph.

Did you find any solution of it?

Regards,

Varshil

0 项奖励
回复

1,381 次查看
joanxie
NXP TechSupport
NXP TechSupport

i.mx95 is still under pre-prodcution, we couldn't share detailed technical information on the public community, pls contact local DFAE to get further support

0 项奖励
回复