Hi, Peter,
As you know that the DSPB56725 does not have on-chip flash, so it starts from on-chip ROM, and start boot-load process, it can boot from external flash with SPI interface, in the case, the SPI of DSPB56725 is master. So you have to write the binary code to the external flash yourself with your own tools, then DSP read code from external SPI flash to internal RAM and run.
Pls download the DSP56724RM from the link:
DSP56725|24-bit Dual-Core Symphony® DSP | NXP
Do you have source code? if you have, pls check if it is based on suite56 tools or Symphony Studio tools. The above tools can generate the *.cld file.
Hope it can help you
BR
XiangJun Rog