First time GDB debug fails

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

First time GDB debug fails

1,756 Views
RobShand
Contributor II

I'm using the S32V234, and am debugging a Linux A53 app on it via Ethernet, using GDB via S32DS.

I'm using the dev board SBC-S32V234

I find that the first time I try to debug after the board powers up, the debug session fails, but on all subsequent attempts, it works.

Does anybody know of a way to avoid this niggle?

Regards,

Rob

Tags (1)
0 Kudos
Reply
2 Replies

1,731 Views
RobShand
Contributor II

Hi BioTICFSL,

Thanks for the suggestion, however, when I try to view that post, I'm told that access is denied? Do I need to log an NXP ticket to resolve my access?

Kind Regards,

Rob

0 Kudos
Reply

1,740 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello RobShand,

 

You should take these considerations,

https://community.nxp.com/t5/Vehicle-Control-and-Networking/S32G-Debug-Considerations/ta-p/1112372?a...

 

Regards

0 Kudos
Reply