Failure Modes in TJA1145A causing Bus Off

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Failure Modes in TJA1145A causing Bus Off

886 Views
vipinrad
Contributor I

What are the physical layer failure modes in TJA1145A that could result in the node going to bus off state. I understand all below will affect comms but not necessarily trigger a bus of state. Any comments?

CAN-H/CAN L open

CAN-H/CAN L/both short to batt

CAN-H/CAN L/both short to gnd

CAN-H short to CAN-L

0 Kudos
Reply
1 Reply

872 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello vipinrad,

I hope all is great with you. Thank you for using the NXP communities.

For further information about the CAN failures of the device, I do recommend reviewing the following application note. 

https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/other/9025/1/AH1309_v1_1_Application_Hin...

I hope this information helps.

Regards,

David

0 Kudos
Reply