FS26 SBC FS1B pin High speed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS26 SBC FS1B pin High speed

859 Views
kjy106906
Contributor IV

I am using SBC FS26.
After booting, FS1B should be raised to High very quickly.
The current SBC Watchdog window setting is 256 ms.
After SBC init, I have to do a Watchdog refresh once to raise FS1B to High.
Therefore, a delay of 200 ms is occurring.
Can I delete this delay?

0 Kudos
Reply
1 Reply

847 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Junyeong,

the FSxB can be released only after the initialization. Please refer to the section 15.3 in the FS26 datasheet, page 28. The initialization is closed by the first good watchdog refresh. Please refer to the section 22.6 in the page 163. in the FS26 datasheet. So unfortunately the FS1B cannot be raised earlier. I apologize for inconvenience.

With Best Regards,

Jozef

0 Kudos
Reply