FS24 and FS26

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS24 and FS26

3,857 Views
nxp96679
NXP Employee
NXP Employee

Hi,

Currently looking from software perspective.

What are the major differences between FS26 and FS24 PMIC?

Do we already have the complex device drivers( AUTOSAR) for FS24 already?

Otherwise, the above change information will be really appreciated, will enable me to adapt the software driver of FS24 based from FS26.

Thanks and Regards,

Sandeep.

0 Kudos
Reply
8 Replies

3,850 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Sandeep,

I hope all is great with you.

In comparison to the FS24 device, the FS26 offers more features. I mean, the number of power supplies, the number of wake up inputs, the register mapping or even the pinout or the package type.

As a brief, the FS24 is not a direct replacement for the FS26 device, and a lot of differences need to be considered when developing SW for it. For further information, please download the corresponding datasheets from your Secure Files.

 

I personally do not think that the AUTOSAR driver is available for the FS24 as it is still in preproduction status. Please let me know if you require further information in order to request it.

I hope this information helps.

Regards,

David

0 Kudos
Reply

3,845 Views
nxp96679
NXP Employee
NXP Employee

Hi David,

Thanks for the response. I have downloaded the documents and will refer further for details.
Had another question, to avoid duplication of software efforts, do you have the information on the timelines on the FS24 AUTOSAR driver and the team which develops those. Because this will enable us to plan accordingly to develop the same or re-use from the provided deliverables.

Thanks and Regards,
Sandeep.

0 Kudos
Reply

3,841 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Sandeep,

Thank you for using the NXP communities. It is our pleasure.

In this case, I will contact the corresponding team for further information.

Upon receiving a response I will contact you immediately. Your patience will be greatly appreciated.

Regards,

David

0 Kudos
Reply

3,834 Views
nxp96679
NXP Employee
NXP Employee

Hi David,
Thank you very much for your prompt response. Really appreciated.
If you have the information available in next weeks, it would be great.
Because we have plans to provide these drivers together with our UWB product NCJ29D6 beginning of next year( mid of 1st quarter 2023).

Thanks and Regards,
Sandeep.

0 Kudos
Reply

3,826 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Sandeep,

I am pleased to contact you again. Your patience is greatly appreciated.

A reply from the NPI team has been sent to you via email.

I hope this information will be useful for you.

Regards,

David

0 Kudos
Reply

3,823 Views
nxp96679
NXP Employee
NXP Employee

Hi David,

Thanks for the action. Yes this was very much useful.

Best Regards,
Sandeep.

0 Kudos
Reply

3,804 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Sandeep,

Thank you for using the NXP community. 

As a brief,  there is no any plan for Autosar Driver till now for FS24.

Have an excellent weekend. 

Regards,

David 

0 Kudos
Reply

3,767 Views
nxp96679
NXP Employee
NXP Employee

Hi David,

Yes that's clear. The generic driver is fine to begin development.

No further questions from my side

Thanks and Regards,
Sandeep.

0 Kudos
Reply