FEC and USB multiplex on mpc5125

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FEC and USB multiplex on mpc5125

1,620 Views
fishhead
Contributor I

I find that the two FECs and the two USBs on mpc5125 are multipexed, so I can't use two FECs and one USB port. Am I right? 

Thank you!

0 Kudos
Reply
1 Reply

1,151 Views
bluehacker
Contributor III

yes.

but if you don't use usb and fec simultaneously, you can support both, for example ,use one 1:2 multiplex chip to connect fec and usb, then switch back and back between them

0 Kudos
Reply