Error writing memory [CCS last error: Connection refused ](CCSProtocolPlugin) Error: invalid input value

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error writing memory [CCS last error: Connection refused ](CCSProtocolPlugin) Error: invalid input value

1,803 Views
avinashh
Contributor III

Hi,

We have P2041 based custom designed board. Initially I was able to connect debugger and initialise SRAM.tcl file for our application. But after programming PBL and uboot bin files to NOR flash, now m not able to initialise SRAM.tcl file and getting error as 

Error writing memory
[CCS last error: Connection refused
](CCSProtocolPlugin)
Error: invalid input value

Can anyone help.

Tags (2)
0 Kudos
Reply
1 Reply

1,440 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Avinash H,

Probably there is problem in RCW, and the target board is in an invalid status, please refine your RCW.

Please refer to the section "8.4 Setting up a remote system to use a JTAG configuration file" in C:\Freescale\CW_PA_v10.5.1\PA\Help\PDF\Targeting_PA_Processors.pdf to use CodeWarrior JTAG configuration file to override RCW on the target board to connect CodeWarrior to the target board to reprogram RCW(PBL).


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply