Error in creating a example MQX v4.1 project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error in creating a example MQX v4.1 project

731 Views
Coacci
Contributor II

Hello!
I'm trying to create a simple MQX v4.1 project, using the example "hello", but right after I build it, it give me this error:
Description Resource Path Location Type
mingw32-make: *** No rule to make target `C:/Freescale/Freescale_MQX_4_1/lib/twrk64f120m.cw10gcc/debug/bsp/intflash.ld', needed by `explicit-dependencies'. Stop. Teste C/C++ Problem

Is there any way to solve it? I've seen indeed the file twrk64f120m.cw10gcc does not exist, how do I generate it?

Thank you!

Coacci_1-1735912113389.png

 

Coacci_2-1735912143836.pngCoacci_3-1735912161835.png

Coacci_4-1735912179493.png

 

0 Kudos
Reply
1 Reply

703 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Coacci:

 

I would suggest you check the below two items.

1.  we need to build the MQX libraries (BSP, PSP,...) before a MQX project.

2.  install the MQX 4.1 in the default folder.

 

Regards

Daniel

 

0 Kudos
Reply