Elastic audio

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Elastic audio

2,403 次查看
kpremendra
Contributor I
Hi,
 
I am using i.MX31ADS board with ATLAS daughter card.
If I play any song on this board the voice quality is elastic. It take almost double time to play compare to PC. It plays good quality vioce if the audio files are encoded with 11khz.
 
Please guide me how to solve/configure the device to get good quality audio.
 
 
Thanx in advance


Message Edited by kpremendra on 2009-01-12 12:03 AM
0 项奖励
回复
3 回复数

1,605 次查看
fabio_estevam
NXP Employee
NXP Employee
Please check the Atlas board checkings:
 

Ø      Atlas switch settings

SW7-1: OFF

SW7-2: OFF

SW7-3: OFF

SW7-4: OFF

SW7-5: ON

SW7-6: ON

SW8-1: ON

SW8-2: OFF

SW8-3: OFF

SW8-4: ON

SW8-5: OFF

SW8-6: OFF

Regards,
 
Fabio Estevam
0 项奖励
回复

1,605 次查看
kpremendra
Contributor I
Thanks a lot ....Fabio Estevam,
 
This settings solved voice problem....
In addition to this I am facing problem with USB port, I could see the kernel message when kernel comes up that USB port detected etc. But when I connect any USB device it does not find... no message in dmesg, no power led indication in USB mass device. Could suggest me what could be the problem.
 
Regards,
Prem
0 项奖励
回复

1,606 次查看
fabio_estevam
NXP Employee
NXP Employee
I suggest you to start a new thread on this USB issue. Also, please describe the Linux BSP version you are using, kernel modules you loaded, command lines, etc.
 
Regards,
 
Fabio Estevam
0 项奖励
回复