ESD protection diode PUSB3F96

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ESD protection diode PUSB3F96

1,223件の閲覧回数
manfredmoeschl
Contributor I

It seems there is a mismatch in the datasheet of PUSB3F96. The breakdown voltage is given with min. 6V and the clamping voltage for positive transients is given with typ. [email protected]. Which one of these two values is correct? Or do I understand something wrong?

0 件の賞賛
返信
1 返信

1,118件の閲覧回数
Bulat
NXP Employee
NXP Employee

Both parameters are correct. As you can see in the datasheet it is not a normal "Zener diode", it is a structure with a very specific snap-back feature. Please take a look at Figure 13 of the datasheet (V-I function) and description on the same page, it explains functionality of the device.

Regards,

Bulat

0 件の賞賛
返信