ESD protection diode PUSB3F96

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ESD protection diode PUSB3F96

1,221 次查看
manfredmoeschl
Contributor I

It seems there is a mismatch in the datasheet of PUSB3F96. The breakdown voltage is given with min. 6V and the clamping voltage for positive transients is given with typ. [email protected]. Which one of these two values is correct? Or do I understand something wrong?

0 项奖励
回复
1 回复

1,116 次查看
Bulat
NXP Employee
NXP Employee

Both parameters are correct. As you can see in the datasheet it is not a normal "Zener diode", it is a structure with a very specific snap-back feature. Please take a look at Figure 13 of the datasheet (V-I function) and description on the same page, it explains functionality of the device.

Regards,

Bulat

0 项奖励
回复