Disabling MC33879 Open Load Detection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Disabling MC33879 Open Load Detection

1,617 次查看
dpendrey
Contributor I

Hi,

I have been using the MC33879 for several years now and it is a great part, but I cannot seem to figure out how to turn the open load detection current off. I am communicating via SPI. I have full control over the outputs of course, but cannot seem to be able to control the open load detection current. Of the two bytes of data required I have tried many different combinations to no avail. Any help in turning it off would be greatly appreciated.

Regards,

David Pendrey

0 项奖励
回复
2 回复数

1,499 次查看
dpendrey
Contributor I

To clarify: I do appear to be able to control the current to an extent.

When I do what the user manual says will turn it on, I can measure a 130uA current to ground on the outputs. When I do what the user manual says will turn it off, I can measure a 12uA current to ground on the outputs.

This is significantly less current, but it is still more than nothing and more than enough to produce a voltage reading.

0 项奖励
回复

1,499 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi David,

I assume you are using bits 15-8 of the 16-bit command to turn on (1) or off (0) the open load detection current.

In low-side configuration, the leakage current should not exceed 5uA:

pastedImage_2.png

In high-side configuration, the leakage current should not exceed 20uA:

pastedImage_3.png

What configuration are you using?

Best regards,

Tomas

0 项奖励
回复