Difference between PJF7992 and PJF7993

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Difference between PJF7992 and PJF7993

2,534 Views
bh117
Contributor I

I'm working on a design and I'm not sure whether to use a PJF7992 or a PJF7993, but I can't find any documentation to be able to distinguish the differences between the two chips. In my limited experiments with them, I've noticed that they behave differently, so is there any information on that?

Thanks!

0 Kudos
Reply
1 Reply

2,472 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Brian,

Actually PJF7992 and PJF7993 are not mass market products supported in this channel, but as far as I know, 7992 is the full version while 7993 is the lite version. For more details , please contact your local Disty. You may refer to the following for details.

Distributor Network | NXP 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply