Debbuger and Programmer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debbuger and Programmer

1,323 Views
jacm
Contributor I

Hi there, 

Has any body program an NXP mcu with a different brand programmer?

I mean, I have a MKE02Z64 VLD4 2N22J XNGL1804K NXP mcu and I would like to use an STLINK-V3SET Debugger/Programmer for STM32. is it possible?

Thanks

 

 

0 Kudos
Reply
1 Reply

1,319 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi jacm,

Please check the release note or user manual, if the MKE02Z64 is in the support device list of STLINK-V3SET Debugger/Programmer for STM32.But generally this type of debugger may limit the MCU model or brand.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply