DSP56720 Boot SPI EEPROM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DSP56720 Boot SPI EEPROM

1,119 次查看
daleulan2
Contributor II

I am wondering if anybody knows what pin /CS should be coming from for a boot SPI EEPROM for the DSP56720? I know this is an older DSP but I have a handful of trays of them I'm trying to use up for a some low-volume DSP products. A bootloader listing would be fine, too, I can read the code pretty easily. Thanks!

0 项奖励
回复
2 回复数

1,067 次查看
daleulan2
Contributor II

Yes, this is perfect. I can hook the EEPROM up based on this and get my PCBs made. I am booting from serial EEPROM in an 8-pin DIP socket initially, then I have a SMD flash on the external data bus as well as a few megabytes of SRAM for delay. I should be able to boot from either the soldered-down parallel flash or the serial EEPROM.

0 项奖励
回复

1,085 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I attach the two files for DSP5672x, hope it can help you

BR

XiangJun Rong