DSP56720 Boot SPI EEPROM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DSP56720 Boot SPI EEPROM

1,129件の閲覧回数
daleulan2
Contributor II

I am wondering if anybody knows what pin /CS should be coming from for a boot SPI EEPROM for the DSP56720? I know this is an older DSP but I have a handful of trays of them I'm trying to use up for a some low-volume DSP products. A bootloader listing would be fine, too, I can read the code pretty easily. Thanks!

0 件の賞賛
返信
2 返答(返信)

1,077件の閲覧回数
daleulan2
Contributor II

Yes, this is perfect. I can hook the EEPROM up based on this and get my PCBs made. I am booting from serial EEPROM in an 8-pin DIP socket initially, then I have a SMD flash on the external data bus as well as a few megabytes of SRAM for delay. I should be able to boot from either the soldered-down parallel flash or the serial EEPROM.

0 件の賞賛
返信

1,095件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I attach the two files for DSP5672x, hope it can help you

BR

XiangJun Rong