DDR4 routing for LS1046A

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DDR4 routing for LS1046A

1,882 次查看
BrunoSenzio
Contributor III

Hello and thanks in advance,

I was looking for DDR4 skew numbers (for length matching on their PCB) as per a customer's request in regards to a design involving the LS1046A and I ended up on Chapter 3.9 of the LS1046A datasheet which explains the timing for SDRAM.

I was wondering if there is additional documentation for this aspect and I thought that finding some reference on the LS1046A could point out to this design rule with Layerscrape.

could it be possible to share some design guidelines for DDR4 with LS1046A if there is any available? (unfortunately I do not have access to additional documentation from Docstore).

Best Regards,

0 项奖励
回复
1 回复

1,871 次查看
r8070z
NXP Employee
NXP Employee

There is application note AN5097, Hardware and Layout Design Considerations for DDR4 SDRAM Memory Interfaces. You can download it from the LS1046A webpage
https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/layerscape-processors/la...

Link to the LS1046A reference board design files you can find at bottom of the LS1046 webpage
https://www.nxp.com/design/qoriq-developer-resources/layerscape-ls1046a-reference-design-board:LS104...
Look for link 'LS1046 RDB Design Files Rev B'

0 项奖励
回复