Custom Firmware image creation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Custom Firmware image creation

ソリューションへジャンプ
1,730件の閲覧回数
Ghouse
Contributor V

Hi, iam using LS1046ardb in a custom card, i want to change the rcw file and build the firmware image with the modified rcw file.

please provide the complete process for generating custom firmware image using modified .rcw file.

Although flex-builder -c rcw -m ls1046ardb can be used to make the "bl2_qspi.pbl",  i want to know if there a procedure to generate the firmware image using .rcw or bl2_qspi.pbl..

0 件の賞賛
返信
1 解決策
1,709件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to file configs/board/ls1046ardb/manifest, rcw_1800_qspiboot.bin is used to generate atf/firmware image.

rcw_qspi="firmware/rcw/ls1046ardb/RR_FFSSPPPH_1133_5559/rcw_1800_qspiboot.bin"

1. Please execute the following command.

$ flex-builder -c rcw -m ls1046ardb

2. Please modify RCW file components/firmware/rcw/ls1046ardb/RR_FFSSPPPH_1133_5559/rcw_1800_qspiboot.rcw for your custom board.

3. Rebuild rcw and atf.

$ flex-builder -c rcw -m ls1046ardb

$ flex-builder -c atf -m ls1046ardb -b qspi

4. $ flex-builder -i mkfw -m ls1046ardb -b qspi

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,710件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to file configs/board/ls1046ardb/manifest, rcw_1800_qspiboot.bin is used to generate atf/firmware image.

rcw_qspi="firmware/rcw/ls1046ardb/RR_FFSSPPPH_1133_5559/rcw_1800_qspiboot.bin"

1. Please execute the following command.

$ flex-builder -c rcw -m ls1046ardb

2. Please modify RCW file components/firmware/rcw/ls1046ardb/RR_FFSSPPPH_1133_5559/rcw_1800_qspiboot.rcw for your custom board.

3. Rebuild rcw and atf.

$ flex-builder -c rcw -m ls1046ardb

$ flex-builder -c atf -m ls1046ardb -b qspi

4. $ flex-builder -i mkfw -m ls1046ardb -b qspi

0 件の賞賛
返信