Cretating a section for MPC5606S graphics RAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cretating a section for MPC5606S graphics RAM

Jump to solution
3,510 Views
fieroluke
Contributor II

Hi everyone,

I am new to the PPC world, so this may be a dumb question, but I would like to know how to define a section for the 160KB on-chip graphics RAM the 5606S features with CW2.9 .The default LCF file only contains sections for regular (ECC) RAM.

I've added the line

graphics_ram : org = 0x60000000, len = 0x00028000

to the MEMORY section, and I defined a group

GROUP : {       graphics : {}    } > graphics_ram

In the code I defined a variable:

#pragma push // save the current state #pragma section RW "graphics"uint8_t buffer[65536];#pragma pop // restore the previous state

But somehow "buffer" still gets allocated in regular internal RAM. What am I doing wrong?

 

0 Kudos
Reply
1 Solution
3,256 Views
fieroluke
Contributor II

Apparently CW only allows #pragma section for initialized data, if an uninitialized section is used in the declspec, the compiler issues an error. In effect, all uninitialized data must go into the (single) BSS segment.

Obviously I don't want all uninitialized data to go into graphics memory, so I put the declaration of the graphics memory buffer into a separate file gfx.c:

uint8_t Vram[240*320];

and in the LCF file I added:

MEMORY{        graphics_ram :     org = 0x60000000,   len = 0x00028000}GROUP : {       .graphicsBSS  (BSS) : { gfx.o (.bss) }               } > graphics_ram

Although the compiler only allows a single BSS segment, the linker allows different BSS segments for different files. At least this seems to work, although I now have to put all graphics descriptor data into separate files. If there is another way of creating and using a separate uninitialized data segment, I'd be glad to know it.

View solution in original post

0 Kudos
Reply
5 Replies
3,256 Views
fieroluke
Contributor II

It seems I need to add a

__declspec(section "graphics")

to the actual variable declaration, which resulted in a "no uninitialized data" error message.

From other posts I have gathered that I need to change the pragma to:

#pragma section data_type "graphics" "graphics"

I'll try that later and report back...

0 Kudos
Reply
3,256 Views
fieroluke
Contributor II

Ok, this seems to work:

GROUP : {       .graphics  (DATA) : {}                  } > graphics_ram
#pragma push // save the current state #pragma section data_type ".graphics" ".graphics"__declspec(section ".graphics") uint8_t Vram[320*240];#pragma pop // restore the previous state

However: although the code works now, the segment is initialized data as it seems, so the binary file is unnecessarily large.

I also tried:

GROUP : {       .graphics  (BSS) : {}                  } > graphics_ram
#pragma push // save the current state #pragma section data_type ".text" ".graphics"__declspec(section ".graphics") uint8_t Vram[320*240];#pragma pop // restore the previous state

Now the segment seems to be uninitialized data, however the compiler wants to put the variable into the initialized section

Hints anyone?

0 Kudos
Reply
3,257 Views
fieroluke
Contributor II

Apparently CW only allows #pragma section for initialized data, if an uninitialized section is used in the declspec, the compiler issues an error. In effect, all uninitialized data must go into the (single) BSS segment.

Obviously I don't want all uninitialized data to go into graphics memory, so I put the declaration of the graphics memory buffer into a separate file gfx.c:

uint8_t Vram[240*320];

and in the LCF file I added:

MEMORY{        graphics_ram :     org = 0x60000000,   len = 0x00028000}GROUP : {       .graphicsBSS  (BSS) : { gfx.o (.bss) }               } > graphics_ram

Although the compiler only allows a single BSS segment, the linker allows different BSS segments for different files. At least this seems to work, although I now have to put all graphics descriptor data into separate files. If there is another way of creating and using a separate uninitialized data segment, I'd be glad to know it.

0 Kudos
Reply
3,256 Views
TomE
Specialist II

How about decalring a global POINTER to the graphics RAM, and have everything use that. Then initialise the pointer in code.

 

Tom

 

0 Kudos
Reply
3,256 Views
fieroluke
Contributor II
That's what I did at first, but when the application is done, I'll have quite a lot of graphics buffers, and I would like the compiler keep track of where which buffer is, instead of keeping track manually.

The DCU2 is able to blend the graphics layers, so there won't be just one or two static (large) buffers, but also many smaller ones of various sizes.

0 Kudos
Reply