Creating files in root file system

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Creating files in root file system

1,601件の閲覧回数
Nich
Contributor III

Hi all,

 

I have a question regarding file system produced by BSP for MPC8308 evaluation board.

I start Linux with "run flashramboot" command in U-Boot. Then in Linux I can successfully create some files in file system. But after restart all files disappear. I tried to create files in different folders: "/", "/home/user", may be somewhere else... and everywhere they disappear after reboot.

I checked in LTIB configuration that "read-only filesystem" option is not enabled... So at the moment I don't understand such behavior...

File system type is ext2.gz

 

Does somebody have some explanation?

0 件の賞賛
返信
2 返答(返信)

1,408件の閲覧回数
TomE
Specialist II

Google for "ext.gz". ".gz" usually means "compressed with gzip". I'd say it is certainly a compressed read-only file system.

 

Type "mount" and see if there are any other partitions mounted that aren't compressed. Otherwise you'll need to add some.

 

Maybe you're meant to plug in an SD card or a USB Memory stick and use that as the read-write file system?

 

Tom

 

0 件の賞賛
返信

1,408件の閲覧回数
Nich
Contributor III

Yes, I have already realized that. Thanks for your response anyway.

0 件の賞賛
返信