Convert Analogue DC to SENT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Convert Analogue DC to SENT

1,274 Views
sergiilevitov
Contributor I

Hi, we are looking for an AD Converter with 2 analogue inputs, to convert DC signal (5V max) to SENT protocol.

Can someone suggest any suitable solution?

0 Kudos
Reply
1 Reply

1,212 Views
lisettelozano
NXP Employee
NXP Employee

Hello Sergii,

Unfortunately, we do not have a product that meets with your specifications.

We have the PCF8591 which is an 8-bit A/D and D/A converter with four analog inputs, one analog output, and a serial I2C-bus interface. You can check more details here https://www.nxp.com/products/analog/interfaces/ic-bus/ic-dacs-and-adcs/8-bit-a-d-and-d-a-converter:P...

I hope this information can be helpful.

Have a great day,

Paulina

0 Kudos
Reply