Connection to Multilink Universal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Connection to Multilink Universal

945 Views
haroldvogel
Contributor II

My system has lost connection to the Multilink Universal device.  The led indicators are on when the system is connected.  The device shows up in the device manager under Jungo - USB Multilink 2.0

pastedImage_0.png

when I try to down load the code to the board

pastedImage_1.png

and

pastedImage_2.png

I have reset the computer (shutting down and restart also tried the re-boot option) but still receive the above error.

I hope that some one can tell me how to get the unit back working.

0 Kudos
Reply
1 Reply

881 Views
haroldvogel
Contributor II

Fixed

0 Kudos
Reply