Configuring SJA1105 using SPI commands

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Configuring SJA1105 using SPI commands

1,849件の閲覧回数
aharoune
Contributor I

Hello All.

I have the following connections in my project.

aharoune_0-1727636757838.png

I want to be able to configure the NXP switch so that any messages to be sent from Port 2 to be routed to Port 3 and 4.
and any messages sent through Port 3 to be routed to Port 2 and 4. and any messages sent through Port 4 to be routed to Port 2 and 3.
Basically I want to be able to use the Connectors on Port 2 and 3 to route and sniff data to and from  EQ6H.

I want to know the SPI commands and static configurations to be configured to the NXP switch.

0 件の賞賛
返信
3 返答(返信)

1,806件の閲覧回数
PavelL
NXP Employee
NXP Employee

Hello,

what version of SJA1105 are you using?

Best regards,

Pavel

0 件の賞賛
返信

1,803件の閲覧回数
aharoune
Contributor I
SJA1105R
0 件の賞賛
返信

1,754件の閲覧回数
PavelL
NXP Employee
NXP Employee

Hello aharoune,

I apologize for late response. There are two tools available for configuring SJA1105:

  1. SDK SJA1110 contains basic support of SJA1105
  2. Python3 tools SJA1105X_CONFIG-GENTOOL and Python2 tools SJA1105X-DEVICE-TOOLS

For basic switch functionality, you need to setup L2 Forwarding Table. Please related chapters in Software user manual for SJA1105P, SJA1105Q, SJA1105R, SJA1105S and AH1704 SJA1105PQRS Application Hints.

This link Solved: SJA1105QEL config - NXP Community might be also useful for you.

Best regards,

Pavel

0 件の賞賛
返信