Code source fo internal clock for NXP S32K146

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Code source fo internal clock for NXP S32K146

1,515件の閲覧回数
sebastien_ledio
Contributor I

Hello,

I am developping SW on S32K146 NXP microprocessor. Actually I use an external cristal for system clock. The SW runs correctly.

Now, I would like to remove this cristal, so use the internal clock, but something does not work.

Someone can help me by give me an source code example to know how configure internal clock without cristal.

By advance, thanks a lot

0 件の賞賛
返信
1 返信

1,468件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Sebastien Le Diouris

The default configuration out of reset has the CPU clocked by the Fast IRC (FIRC_CLK), so actually, you should be able to run the MCU without an external crystal. are you setting up the external clock in your startup file? could you clarify what part doesn't work, or what behaviour are you seeing?


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------

0 件の賞賛
返信