Cockpit console issue with yocto build Image

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cockpit console issue with yocto build Image

6,389件の閲覧回数
bckpoojary
Contributor I

Hi,

I'm facing cockpit browser console issue in yocto builded image(6.1-mickledore) for i.mx8M nano ,I have added below mentioned cockpit image recipes into conf/local.conf file .but after the successful installation ,when accessing from browser using https://<ip_address>:9090 its showing below error,i have tried from updated browser also but facing same error,can anyone please help me on the issue?

 

This web browser is too old to run the Web Console (missing selector(:is():where()))

 

#IMAGE_INSTALL:append = " cockpit cockpit-pcp cockpit-tuned cockpit-shell cockpit-systemd cockpit-users cockpit-kdump cockpit-sosreport cockpit-selinux cockpit-playground cockpit-dashboard cockpit-bridge cockpit-ws cockpit-desktop

 

Thank you

 

0 件の賞賛
返信
2 返答(返信)

6,359件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello,

 

Could you please share the steps that you did to compile your image?

Also, could you please share the processor you are using?

 

Thank you.

 

Best regards,

--... ...--

Salas.

0 件の賞賛
返信

6,329件の閲覧回数
bckpoojary
Contributor I

Hi @Manuel_Salas ,

Thanks for your response.

I'm using i.mx8M Nano lpddr4 EVK with "imx-image-multimedia" image to compile.

added local and bblayer configuration file in below attachments.

 

Thank you

Regards

Bharath GC

 

 

0 件の賞賛
返信