Hi Sivahari,
Thanks for your reply. From your point i understood that Standby mode and LPOFF mode is common for both Failsafe and Main state.
[A] Correct.
But we need to give any wake events(Wake1, Wake2, GPIO1, GPIO2, LDT and CSB pin) to bring SBC from Standby mode to "Default M_OTP Loading" right as it was mentioned in State diagram (15.1 simplified State diagram)?
[A] Yes, correct.
And once it reached to "Default M_OTP Loading" from Standby mode then what about the LBIST test and Fail safe register configurations?
Whether LBIST perform again and Fail safe register settings load with default values?.
[A] The Fail-Safe will start from the beginning. Please refer to the window in the top of the Fail-Safe section. Deepening on the LBIST_STDBY_OTP [7:0] register settings the LBIST will be performed or bypassed if FS26 is coming from Standby mode.

With Best Regards,
Jozef