Clarifications required on SBC FS2613

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Clarifications required on SBC FS2613

1,447 次查看
Sivahari
Contributor I

Hi Team,

I am working on SBC module development. Part number(MFS2613AMDA6_REV_A).

I have gone through SBC product datasheet and I have clarifications on following points.

1. In simplified functional state diagram, Is that Fail safe state and main state has common Standby mode and LPOFF mode or having separate one for each state?

2. I saw there is a possibility to transit the SBC state from FS Standby mode to FS Init phase by Wake events and through SBC main sate Normal mode. So, is that correct? and do we have other alternate options to transit the SBC State directly from Standby mode to init Fs state?

0 项奖励
回复
3 回复数

1,430 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Sivahari,

1. In simplified functional state diagram, Is that Fail safe state and main state has common Standby mode and LPOFF mode or having separate one for each state?

[A] Same. Please refer to the registers by which the FS26 will transfer to Pre-Standby mode in Fail-Safe (Standby Power Down sequence in Main) and to Pre-LPOFF mode (LPOFF Power Down sequence in Main). You can transit to Pre-modes in the Fail-Safe and the FS26 will stay in Normal mode. 

2. I saw there is a possibility to transit the SBC state from FS Standby mode to FS Init phase by Wake events and through SBC main sate Normal mode. So, is that correct? and do we have other alternate options to transit the SBC State directly from Standby mode to init Fs state?

[A] No, this is not possible. From Standby mode you need to start from the "Default M_OTP Loading". To INIT FS the FS26 will switch automatically from Pre-Standby mode, if FS_LP_REQ [7:0] will not be set to 0x55 within 10 ms after FS_LP_REQ [7:0] set to 0xAA.

With Best Regards,

Jozef

0 项奖励
回复

1,427 次查看
Sivahari
Contributor I

Hi Jozef,

Thanks for your reply. From your point i understood that Standby mode and LPOFF mode is common for both Failsafe and Main state.

But we need to give any wake events(Wake1, Wake2, GPIO1, GPIO2, LDT and CSB pin) to bring SBC from Standby mode to "Default M_OTP Loading" right as it was mentioned in State diagram (15.1 simplified State diagram)?

And once it reached to "Default M_OTP Loading" from Standby mode then what about the LBIST test and Fail safe register configurations?

Whether LBIST perform again and Fail safe register settings load with default values?.

0 项奖励
回复

1,416 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Sivahari,

Thanks for your reply. From your point i understood that Standby mode and LPOFF mode is common for both Failsafe and Main state.

[A] Correct.

But we need to give any wake events(Wake1, Wake2, GPIO1, GPIO2, LDT and CSB pin) to bring SBC from Standby mode to "Default M_OTP Loading" right as it was mentioned in State diagram (15.1 simplified State diagram)?

[A] Yes, correct.

And once it reached to "Default M_OTP Loading" from Standby mode then what about the LBIST test and Fail safe register configurations?

Whether LBIST perform again and Fail safe register settings load with default values?.

[A] The Fail-Safe will start from the beginning. Please refer to the window in the top of the Fail-Safe section. Deepening on the LBIST_STDBY_OTP [7:0] register settings the LBIST will be performed or bypassed if FS26 is coming from Standby mode.

JozefKozon_0-1742818644063.png

With Best Regards,

Jozef

0 项奖励
回复