Can I use old date code for MRF9045LSR1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I use old date code for MRF9045LSR1

1,277 Views
sakri_ahmad
Contributor I

I have MRF9045LSR1  with date code 1228, 1229 (year 2012). 

Can I use this device for my product?

Labels (1)
  • RF

0 Kudos
Reply
1 Reply

1,176 Views
LPP
NXP Employee
NXP Employee

Yes. You can use this device.

For  NXP  devices  offered  with  a  gold lead finish,  adequate solderability is ensured in the end application. If no harmful contamination comes into contact with the components, there is no aging process in the parts and they will have a almost unlimited shelf life span.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply