Can I sent a rbga 32bpp file to LVDS 24bpp ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I sent a rbga 32bpp file to LVDS 24bpp ?

743 Views
fs31
Contributor I

Hello,

I try to display a test picture on my TFT but have some wrong colors.

I generated a raw picture, based on a PNG file (with alpha channel) using ffmpeg.

ffmpeg -i testpattern.png -vf scale=1280:480 -s "1280x480"   -vcodec rawvideo -f rawvideo -pix_fmt brga  testpattern.raw

Then, on the imx terminal, I do:

cat testpattern.raw > /dev/fb0

Basic colors area are ok ( full red, blue, green, yellow, turquoise, pink, black and white are ok  = all area with color made of  0 or FF in RGB fields)

All shade area or photo have wrong colors: example: a large red to black share because 4 little red to black share.

fbset give this:

mode "1280x480-59"

        geometry 1280 480 1280 960 32

        timings 23381 16 54 8 40 8 4

        accel false

        rgba 8/16,8/8,8/0,8/24

endmode

My concern is that maybe the 32bpp of the file cannot be sent on the LVDS (24bit single channel). can it be that?

I tried

fbset -rgba 8/16,8/8,8/0,0/0

I have a kind of quick blink on the display but no effect. Also fbset keeps giving same as before (no modification).

If not, other ideas ?

Best regards,

(I'm new here, I hope I'm clear enough).

0 Kudos
Reply
0 Replies