CLRC663 transmitted power

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CLRC663 transmitted power

1,088件の閲覧回数
jessie_yan
Contributor I

what is the maximum transmitted power on the CLRC663 when you are using 3.3V and only driving TX1? 

ラベル(1)
  • RF

タグ(1)
0 件の賞賛
返信
1 返信

968件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Jessie Yan,

    When you deisign project based on CLRC663,  TVDD pin should be supplied 3.3V~5V. Transmitting current is Max 250mA or 350mA, which is determined by CLRC663 part number. you can get it from datasheet.

Have a nice day!

Weidong.

0 件の賞賛
返信