CAN Transceiver compatible with ISO 11992

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN Transceiver compatible with ISO 11992

2,303 Views
lukas0
Contributor I

Dear Support,

 

I'm looking for a ready to use CAN Transceiver compatible with ISO 11992 (Road vehicles — Interchange of digital information on electrical connections between towing and towed vehicles) which operates with different bus levels than standard CAN bus:

The logic “recessive” state is specified by the following voltage levels of CAN_H and CAN_L:
VCAN_H = 1/3 Vs
VCAN_L = 2/3 Vs
The logic “dominant” state is specified by the following voltage levels of CAN_H and CAN_L:
VCAN_H = 2/3 Vs
VCAN_L = 1/3 Vs

where Vs is nominal 24 V in heavy vehicle.

Is TJA1055 suitable for this application?

 

 
0 Kudos
Reply
1 Reply

2,284 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello lukas0,

I hope all is great with you. Thank you for using the NXP communities.

Unfortunately NXP does not offer transceiver that complies with the ISO 11992.

Please accept my apologies for any inconvenience this situation might cause.

Regards,

David

0 Kudos
Reply