Bootloader code for the MPC5604

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bootloader code for the MPC5604

5,023 Views
bryanwade
Contributor I

I'm just getting started Freescale products so please forgive me if I'm missing something obvious. Is there any example bootloader code available for the the MPC5604P or similar?

Ultimately I plan to update application code via Flexray, but a UART or CAN example would be a good starting point.

Thanks.

3 Replies

3,413 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

attached you will find draft of my application note. Hope it will be useful.

Lukas

3,413 Views
Stevanatto
Contributor II

I will use this code too. Thank you.

0 Kudos
Reply

3,413 Views
gangzhou
Contributor II

Tkank you for sharing the bootloader code.I want to write a bootloader for MPC5644A according to your code.But,the program can not run properly.And ,stop at function EXCEP_DefaultExceptionHandler().Whether I must write some command files in my project like

"t32" file  in your project or not? How should I do?

0 Kudos
Reply