Pls refer to below answers based on confirmation internally:
the engineer used to recommend BGU7044, it is a device designed for TV Set-Top Box applications. It has 75 Ohm input and output impedance. It is an inverting amplifier.
But, it has lower Gain (14dB vs 31dB) and it has different pinout than BGA2870.
this part is "not for new designs", either.
https://www.nxp.com/part/BGU7044#/
2) NXP does not provide SPICE models for these amplifiers but S-parameters only.
BGA2870 S-parameters can be found in the device product pages.
https://www.nxp.com/products/radio-frequency/rf-amplifiers-low-medium-power/low-noise-amplifiers-lna...
MODELS
3: "115" only indicates the packing of this part: Packing: REEL-Reel 7" Q1/T1
BGA2870,115
Pls refer to the packing letter of this part:
https://www.nxp.com.cn/docs/en/supporting-information/Packing_Letter_code.pdf
Hope it helps, thank you.
Pls let me know if you have further questions.
Have a nice day.