Auto detect the CAN baud rate

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Auto detect the CAN baud rate

1,372 Views
jqch
Contributor I

I can configure the baud rate to 250K or 500K respecitvely. but I need dyanmically configure the buad rate according to the baud rate which other node (say master node) is using. I tried to set CAN in Listen Only mode, and configure a rate as well as enable CAN module, then I was tring to read CANRXERR register value, how can I read the value?  does any one have the experience?

Thanks

0 Kudos
Reply
1 Reply

1,088 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

what is the device you are referring to?

Regards,

Petr

0 Kudos
Reply