Assistance with Enabling USB0 Interface for LTE Module on i.MX8M Mini EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Assistance with Enabling USB0 Interface for LTE Module on i.MX8M Mini EVK

921 Views
dhananjay896
Contributor I

Dear NXP, 

I am currently using the i.MX8M Mini LPDDR4 EVK, where I have flashed the prebuilt Linux image. The kernel version of the image is 6.6.36-lts-next-gd23d64eea511.

dhananjay896_0-1737949321542.png

I am attempting to connect an LTE module (SIM7600G-H) to the EVK. After consulting with the LTE module vendor, I was informed that enabling the USB0 interface is required for proper communication with the module.

dhananjay896_1-1737949988959.png

Could you kindly point me to any relevant documentation or suggest the steps necessary to connect and configure the LTE module with the i.MX8M Mini EVK?

NOTE: I have attached the LTE module image for your reference.

Thanks for your support.

Regards,

Dhananjay Gupta

Tags (1)
0 Kudos
Reply
1 Reply

894 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

You need to rework the EVK since USB signals are not connected to M.2 connector and configure it, you can use our device tree as reference.

JorgeCas_0-1738098887699.png

Best regards.

0 Kudos
Reply