Alternative Competitive Devices from NXP portfolio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Alternative Competitive Devices from NXP portfolio

2,752 Views
b18740
NXP Employee
NXP Employee

Would like the technical expertise to help find an alternative competitve part from our existing portfolio to compete/be compatible with below two competition part with same functionalities and features set. Any device suggestion?

 

(1)Analog Devices Low Voltage Controller for Touch Screen (AD7879-1ACPZ-RL). Function is 12bit AD with driving 4-wire resistive touch screens,and I2C communication interface. (http://www.analog.com/media/en/technical-documentation/data-sheets/AD7879_7889.pdf)

(2)Linear Technology, White LED Driver with integrated Schottky in SC70 and 2mmx2mm DFN (LT3491ESC8) Function is drive up to six white LEDs, and use to dirve LCD’S LED. (http://cds.linear.com/docs/en/datasheet/3491fa.pdf)

0 Kudos
Reply
1 Reply

2,653 Views
guoweisun
NXP TechSupport
NXP TechSupport

Unfortunately for these devices,NXP doesn't have replacement part.

0 Kudos
Reply