Alternative Competitive Devices from NXP portfolio

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Alternative Competitive Devices from NXP portfolio

2,751 次查看
b18740
NXP Employee
NXP Employee

Would like the technical expertise to help find an alternative competitve part from our existing portfolio to compete/be compatible with below two competition part with same functionalities and features set. Any device suggestion?

 

(1)Analog Devices Low Voltage Controller for Touch Screen (AD7879-1ACPZ-RL). Function is 12bit AD with driving 4-wire resistive touch screens,and I2C communication interface. (http://www.analog.com/media/en/technical-documentation/data-sheets/AD7879_7889.pdf)

(2)Linear Technology, White LED Driver with integrated Schottky in SC70 and 2mmx2mm DFN (LT3491ESC8) Function is drive up to six white LEDs, and use to dirve LCD’S LED. (http://cds.linear.com/docs/en/datasheet/3491fa.pdf)

0 项奖励
回复
1 回复

2,652 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Unfortunately for these devices,NXP doesn't have replacement part.

0 项奖励
回复