Adding new board to NXP flexbuild

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Adding new board to NXP flexbuild

867件の閲覧回数
Avyukt_BLD
Contributor I

I am trying to build a Debian based system for the Olimex imx8mp evaluation board using the NXP Flexbuild tool. Since this is a 3rd party board so I have to add the board configuration file manually and I followed the steps as specified in the flexbuild document: 

https://docs.nxp.com/bundle/UG10155/page/topics/how_to_add_a_new_board_in_flexbuild.html

I added the .conf file from the meta-freescale-3rdparty repository: https://github.com/Freescale/meta-freescale-3rdparty/blob/master/conf/machine/olimex-imx8mp-evb.conf

after following the steps and adding the .conf file for the board, I tried building the firmware but got this error:

MACHINE: olimex-imx8mp-evb
/home/parth/flexbuild/configs/board/olimex-imx8mp-evb.conf: line 7: require: command not found

According to this error message, the syntax of the .conf file for the board is not right, that's why its not right.
can anyone please suggest how to resolve this issue?

0 件の賞賛
返信
1 返信

851件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @Avyukt_BLD 

I hope you are doing very well.

The NXP Flexbuild tool is just for NXP boards, the third party board are not supported.

 

Best regards,

Salas.

0 件の賞賛
返信