AN142522 RF Amplifier for NXP Contactless NFC Reader IC's

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AN142522 RF Amplifier for NXP Contactless NFC Reader IC's

1,578件の閲覧回数
amighri
Contributor II

Hi,

Does NXP provides Amplifier circuits for NFC Readers ? 
How should be this circuits connected with the reader ? is there any hardware guide for designing an amplifier circuit and connecting it to the reader ? 
 
Thanks
 
0 件の賞賛
返信
3 返答(返信)

1,529件の閲覧回数
amighri
Contributor II

Hi @Kan_Li  , 

Does using an amplifier circuit improve the range of the reading operation distance between the tag and the reader?

Thanks in advance. 

0 件の賞賛
返信

1,520件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @amighri ,

 

Yes, that can be done.

Please be aware that the amplifier delivers more RF power, but it does not provide a better coupling. Thus, the cards might be powered at a larger distance, but the Rx might not be able to receive the card response in that case. 

 

Hope that makes sense,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,548件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @amighri ,

 

Please kindly refer to https://www.nxp.com/docs/en/application-note/AN1425_AN166510.zip for details, in which you may find an application note on this topic as well as an excel file for calculation the parameters.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信