AFT09MS031N ADS DC Simulation Issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AFT09MS031N ADS DC Simulation Issues

1,286 Views
MRHUANG
Contributor I

Why, when performing the static operating point simulation of AFT09MS031N LDMOS using ADS, did we find that the static current was in the nA range? First of all, it should be noted that there are no issues with the circuit diagram or the installation package components.

0 Kudos
Reply
4 Replies

1,264 Views
juyujayav
Contributor I

Firstly, ensure that the biasing conditions are appropriately set for the LDMOS. If the gate voltage is too low or not properly configured, it could lead to minimal current flow. Additionally, check the supply voltage to ensure it meets the required levels for the device to operate correctly.

0 Kudos
Reply

1,246 Views
MRHUANG
Contributor I
This is certainly no problem. I suspect it's a model issue or that the latest model is incompatible with the ADS2024 version.
0 Kudos
Reply

1,226 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello, did you install the RF High Power Model Kit 2025?

Rev 3.1 (for ADS2016, ADS2017, ADS2019, ADS2020, ADS2022, ADS2023, 2024 and 2025)

https://www.nxp.com/products/radio-frequency-rf/rf-high-power-models/models-for-ads-keysight-advance...

 

0 Kudos
Reply

1,026 Views
MRHUANG
Contributor I

sure Otherwise, the simulation will not be successful.

0 Kudos
Reply