AFIC10275N Airfast RF LDMOS Wideband Integrated Power Amplifier

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AFIC10275N Airfast RF LDMOS Wideband Integrated Power Amplifier

1,247件の閲覧回数
abhat
Contributor I

Hello,

I am very interested in evaluating the AFIC10275N power amplifier for an on-going prototype development. I would appreciate any help in getting started with this part in a laboratory environment, that includes ordering the evaluation boards, biasing-sequencing circuits and requirements for Drain/Gate supply voltages and instructions for lab-testing.

Regards,
Arvind

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 返信

918件の閲覧回数
Wlodek_D_
Senior Contributor II

Dear Arvind Bhat,

I've found that your question has been already answered directly in Service Request you opened on 17-Jun 2015.

The answer was:

"In case of AFIC10275N power amplifier there is have possibility to order test board (test fixture).

You need to contact our Authorized Distributor - in US it is Richardson RFPD, e-mail: rfpdsales@arrow.com or phone: (800) 737-6937. They will place purchase order for you at Freescale. Please refer to device Part Number (AFIC10275N and working frequency range - board for 1090 MHz Applications is available). "

I believe the SR advice was helpful and you successfully started your project.

Best regards,

Wlodek_D.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信