ADS high power model application

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADS high power model application

2,210 Views
ryanfeng
Contributor I

I can't use ADS high power model: A2T07H310-24S in ADS2008U2? How to solute this problem? Is this model available in 2008U2?

Labels (1)
  • RF

0 Kudos
Reply
2 Replies

2,077 Views
LPP
NXP Employee
NXP Employee

We have no A2T07H310-24S model for ADS2008U2.

A2T07H310-24S ADS model that is provided can be used for ADS2009U1, ADS2011, ADS2012, ADS2013, ADS2014, ADS2015 and ADS2016. It doesn't work with ADS208U2.

Best Regards,

Pavel

0 Kudos
Reply

2,077 Views
ryanfeng
Contributor I

Hi

The A2T07H310 model still can not be used in ADS2011_10. Do you guys have any list such as which model can not be used in ADS20xx...

0 Kudos
Reply