ADC Function WCT-15WTXAuto

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC Function WCT-15WTXAuto

2,406 Views
devinpark
Contributor II

Hi Experts,

Recently, WCT-15WTXAuto EVM was released on the last October and we can find its schematic and SDK(v3.1).

In adc.h of the SDK, we can see following code. BTW, for example, its schematic(rev B2) uses AN_A5 forVRAIL and AN_B7 for TEMP4.

 I checked the whole source code but I think the code using ADC is wrong.

is the SDK just a beta version? otherwise is my thinking not correct??

typedef enum
{
ADC_MISC_CHANNEL_VRAIL_INDEX = 0,
ADC_MISC_CHANNEL_INPUTCURRENT_INDEX,
ADC_MISC_CHANNEL_VRAILA_INDEX,
ADC_MISC_CHANNEL_VBAT_INDEX,
ADC_MISC_CHANNEL_IPEAK_INDEX,
ADC_MISC_CHANNEL_TEMP1_INDEX,
ADC_MISC_CHANNEL_TEMP2_INDEX,
ADC_MISC_CHANNEL_TEMP3_INDEX,
ADC_MISC_CHANNEL_TEMP4_INDEX,
ADC_MISC_CHANNEL_NUM
}ADC_MISC_CHANNEL_E;

.

BR,

Devin

Labels (1)
0 Kudos
Reply
1 Reply

2,299 Views
devinpark
Contributor II

Hi,

I found that the enumeration is related with adc_clist1/2/3/4 & sdis. So now I think the code is correct.

BR,

Devin

0 Kudos
Reply