9S08qd2 Development problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

9S08qd2 Development problem

757 Views
nasim
Contributor I

I am using Code Warrior IDE version 6.3 (although help->about shows 5.9.0) and P&E Multilink BDM debugger .my problem is that when I Load the program it shows valid RAM address up-to 0x15f  were as the prm file has the allocation up-to 0xff. The controller registers are also not behaving normally.I think there is some problem with the header file for the controller.

Please advice

Regards

Nasim

0 Kudos
Reply
0 Replies