56f8023 - external Crystal oscilator?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

56f8023 - external Crystal oscilator?

Jump to solution
2,678 Views
VdS
Contributor I
Hello.
 
Can I use an external crystal oscillator with 56f8023? It seems in the datasheet this is posible. However what is unclear to me is which pins are used for it? They are supposed to be marked in the pinout diagram as XTAL and EXTAL but they are nowhere to be found?!
 
I also searched for an eval board and went trough the GPIO description, but no success.
 
Any ideas?
 
--
Alban Edit: Product must appear in subject line + descriptive subject.
 
 

Message Edited by Alban on 2007-04-17 10:25 AM

0 Kudos
Reply
1 Solution
1,754 Views
william_jiang
NXP Apps Support
NXP Apps Support
This device does not support external crystal, but only external clock. If you want to connect external crystal, please choose 56F8025/36/37.

View solution in original post

0 Kudos
Reply
1 Reply
1,755 Views
william_jiang
NXP Apps Support
NXP Apps Support
This device does not support external crystal, but only external clock. If you want to connect external crystal, please choose 56F8025/36/37.
0 Kudos
Reply