33771B SPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

33771B SPI

1,578 Views
Yongdong
Contributor I

Hi NXP Team

    Can the 33771BT series support SPI? If it is not supported, why is there a SPI_COM-EN pin?

0 Kudos
Reply
1 Reply

1,547 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Some parts can support SPI and the detail information please kindly refer to the below:

fangfang_0-1733708949966.png

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos
Reply