Multisensor freedom shield board with FXLS8974CF, NMH1000 and MPL3115A2S sensors.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multisensor freedom shield board with FXLS8974CF, NMH1000 and MPL3115A2S sensors.

Multisensor freedom shield board with FXLS8974CF, NMH1000 and MPL3115A2S sensors.

I have designed an Evaluation board with three NXP sensors. Please find the design files attached. I have tested standalone mode of the NMH1000 magnetic sensor, and it worked correctly. This way I have confirmed, that the power supply to the NMH1000 and output pin for detecting magnetic field presence are correctly routed.

For the NMH1000 standalone test, mount the FRDM-STBC-FNM03 on top of FRDM-K22F freedom board and set the jumpers as follows.

J5 1-2

J6 2-3

By the J14 and J15 you can choose threshold and output data rate respectively. For testing you can leave both not connected. 

Then you can apply and remove magnetic field close to the NMH1000 chip and see change in logic level on the OUT pin. 

ラベル(1)
添付
評価なし
バージョン履歴
最終更新日:
3 週間前
更新者: