UWB Secure Ranging (FIRALITE)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UWB Secure Ranging (FIRALITE)

3,237 Views
kuldeep
Contributor I

I need some help on secure ranging on SR150. I’m facing an issue when running Firalite secure ranging demo from UWBIOT_SR150_v04.02.01_MCUx. On debugging further I see a failure to select FIRALITE ADF,

The below call fails.

// initiator: select ADF LOG_I("initiator: select ADF");

se_status = Se_API_SelectADF(optsA, oid_entries, oid_entries_count, &selectAdfResponse);

ENSURE_OR_GO_EXIT(se_status == SE_STATUS_OK);

From readme for Firalite secure randing demo, below are the prerequisites

- SE051W should be connceted to host Refer :ref:`board-se051w`

- SR150 should be bound to SE051W. Refer :ref:`sr150-demo-binding`

- Perform the ADF provisioning Refer :ref:`firalite-adf-provisioning`

- Once ADF provisioning sucessful we can run the demo_fl_initator.

 

I was able to do the binding successfully. I could not find any information on firalite-adf-provisioning in SDK or in NXP site documentation. I suspect, The failure to select ADF is because of not doing firalite-adf-provisioning. Can you please help share the steps/demo code for firalite-adf-provisioning?

0 Kudos
Reply
3 Replies

1,176 Views
two_cloud
Contributor I

When performing operations based on firalite-adf-provising, I have the following questions:
1. How can I burn the se_VCOM firmware? Is it through DK6Programmer.exe?
2. After running the JRCPProxyConsole.exe -c COM44 command, no feedback is displayed in PowerShell.

3. The JCShell tool is not available.

0 Kudos
Reply

1,855 Views
Pierre0811
Contributor I

Hello,

I have the same problem as Kuldeep; is there now a place where the information is accessible, or did we need to be contacted by NXP to solve this problem?

Regards

0 Kudos
Reply

3,215 Views
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi @kuldeep ,

Hope you are doing well. You will be contacted directly.

Have a nice day!

Regards